Description

Version

Info

Supported Models

Keysight N7874A PXI e/USB Vector Network Analyzer Calibration Application Software

E.03.00

Readme

M9370A, M9371A, M9372A, M9373A, M9374A, M9375A, P9370A, P9371A, P9372A, P9373A, P9374A, P9375A

What's New!

N7874A PXIe/USB Vector Network Analyzers Calibration Application E.03.00

What's New

New UUT Models and Options Supported

  • Supports the new Keysight Streamline series VNAs: P9370A, P9371A, P9372A, P9373A, P9374A, and P9375A

New Test Equipment

  • New D-series N4691D ECal module is now supported. It will be the recommended model.
  • PNA-X network analyzers N5245B, N5247A, and N5247B are now supported. The N5245B is the recommended model.

New Features and Enhancements

  • Uncorrected Error Terms Performance Test: This test has been enhanced to reduce the number of connections needed. The new method uses the unknown thru functionality of the VNA.
  • Flexible Channel Assignment logic: Tests using a power meter and power sensor will now use Flexible Channel Assignment logic. This logic will identify the channel that a power sensor is connected to using the ability of "smart" sensors such as the N848xA series power sensors to report their full model and serial number.