Description

Version

Info

Supported Models

Keysight N7832A Power Meter Calibration Application Software

E.04.04

Readme

N1911A, N1912A, N1913A, N1914A, N8262A

What's New!

Version E.04.04 (July 2017)

  1. Removed the LXI Finder tool used during the detection of the N8262A power
    meters. Instead operators will now be presented with a dialog box to
    enter the IP address of the N8262A. Note that the default form of a
    hostname for the N8262A is A-N8262A-XXXXX or K-N8262A-XXXXX where XXXXX is
    the last 5 digits of the serial number. The IP address of the N8262A may
    be obtained through the Agilent/Keysight IO Libraries Suite.
  2. Fixed an issue with the Absolute Accuracy report header where the test
    limit column was missing a +/-.
  3. When entering the power meter accuracy in the Reference Output Power
    dialog that is displayed prior to the 1 mW Power Reference Level
    Performance Test and 1 mW Power Reference Adjustment, a warning message
    is now displayed if the accuracy entered is not within the recommended
    range identified in the help file.