Description Version Info Supported Models

Agilent N7805A E6601A Wireless Communication Test Set Calibration Application Software

E.05.00

Readme E6601A
 What's New
Return to download page

Version E.05.00 (December 2007)
Version 5.0 (Version E.05.00) adds performance tests for the new TD-SCDMA and cdma2000/1xEV-DO test capability of the E6601A Wireless Communications Test Set.

  1. Low Power and High Power Coupler Calibration
    NOTE: Although the above calibration procedures are added to the Performance Verification test plan, they are not required for a complete performance verification. These procedures peform calibrations required by several later tests, and executing them will make the overall calibration process more efficient.
  2. Compatible with TME version E.02.05 or later
  3. Adds the following performance tests:
    • TD-SCDMA format (4 tests)
    • cdma2000/1xEV-DO RF An (7 tests)
    • Fast device tune (3 tests)
    • VSWR (1 test)
    • General purpose digital modulation quality (1 test)
    • Extend testing > 2GHz for
  4. cdma2000, W-CDMA
    • Modified 21 existing tests to cover new frequency bands <2 GHz
  5. GSM, GPRS, EGPRS, W-CDMA, cdma2000
    • New measurement reports for changes and new tests above

 

Return to download page